{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Updating DST Settings for Meter Clock using ION Setup

Issue
Updating daylight savings time (DST) settings for PowerLogic ION power meter clocks via ION Setup.

Product Line
PM8000
ION8650
ION8600
ION7650, ION7550
ION7600, ION7500, ION7400

Environment
ION Setup 3.0

Cause
Updating DST Settings for meter clock using ION Setup.  This is much easier than using ION Designer, in particular, there is no need to predetermine the DST Start and End dates.

Resolution

- Connect to meter using ION Setup. (See ION Setup user guide)

- Determine the physical location of device and the respective Time Zone (for UTC adjustment).

- Using Setup Assistant to set the time zone setting for the clock module.


Setup assistant
- Edit the Timezone Register, making sure both Automatically adjust clock for daylight saving changes and Update all available daylight saving dates are checked.

Timezone selection
- The DST Settings should now be updated

Setup assistant

- Edit remaining settings for the clock module (refer to Time Synchronization & Timekeeping technical note).

Schneider Electric Global

Attachment(s)
TimeSynchronization&Timekeeping-70072-0111-14.pdf [318.92 KB]