Issue
Diagram for wiring an ACE-959 4-Wire Modbus RS485 I/F Module as 2-Wire.
Product Line
ACE-959, Sepam
Environment
Sepam Communications
Cause
The ACE959 interface provides an electrical interface between Sepam™
and a 4-wire RS485 communication network. It is the main network cable
branching box for connecting a Sepam with a CCA612 cable
Resolution
See the diagram below for details on the connection from a 4-wire RS485 to 2-wire RS485 connection using the ACE-959
Attachments
The attachment is the PDF version of the diagram above.
Original article# 3688
All content © 1992-2008 Schneider Electric
Legacy KB System (APS) Data: RESL185609 V2.0
Related ranges: ACE 9XX, Cabling and connection accessories
Released for:Schneider Electric Global