Goals and Symptoms
How to update multiple loadables in ProWORX NxT
Facts and Changes
All versions of ProWORX NxT
Causes and Fixes
'ProWORX NxT' does not allow the update of multiple loadables at the same time. If more than 1
loadable needs to be updated, the update must be performed one at a time.
The following example updates the ESI loadable which also includes the NSUP loadable.
- Open the project.
- Click on 'Configuration' from the top menu bar and select 'Configuration'.
- Click on 'User Loadables'
- Click on first loadable to be updated (i.e., NSUP) in the Loadables in database window.
- Click on the Update button.
- Find the the executable file (i.e., NSUP.exe) and select it.
- Click on the OK to close the Select Loadable File window.
- Click on the OK in the 'Update Successful' message box.
- Click on the OK to save the changes and to close the Controller Configuration window.
- Repeat the process to update the next loadable. (i.e., ESI)
Released for:Schneider Electric Global