{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
171CCC9x0x0 M1E Processor 984LL Exec. Upgrade to v.1.30

Issue
The purpose of this resolution is to inform Momentum M1E users that the 984LL Exec. has been upgraded to version 1.30.

A modification was made to the 984LL Exec version 1.30 that allows users to control the retransmission timer and TCP socket time-out when performing MSTR Read multiple registers and Write multiple register operations.

Further details of this enhancement are described in the attachment below.


Product Line
Momentum
171CCC98030
171CCC96030
171CCC98020
171CCC96020

Note: It is recommended to power cycle the M1E immediately after downloading an Exec.


Resolution
Install Exec version 1.30 to access this new feature. It was not being considered for the IEC firmware at the time this Resolution was published (Aug 2009).
Although this enhancement is supported by ProWorx NxT, ProWorx32 and Concept programming software, it is not supported in the Concept MSTR DX Zoom screens at this time. Resource files are available (see attachments) for ProWorx NxT and ProWorx32.

Attachments

  • Description of new feature to the 984LL Exec version 1.30
    M1_v1.30_Resolution.zip
  • ProWORX 32 resource file UCS
    MSTR_ucs.zip
  • ProWORX NxT resource file URF
    Mstr_urf.zip


Legacy KB System (APS) Data: RESL199702 V1.0, Originally authored by DaDz on 08/25/2009, Last Edited by DaDz on 08/25/2009
Related ranges: Modicon Momentum

Schneider Electric Global

Attachment(s)
MSTR_ucs.zip [1002 Bytes]
M1_v1.30_Resolution.zip [97.68 KB]
Mstr_urf.zip [1.63 KB]