{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
140NOC77101 Explicit Messaging CIP Modbus Object Read Example

Issue
The attached document is a CIP Modbus Object Read example for a 140NOC77101 using the MBP_MSTR block to read from another Quantum 140NOC77101.


Product Line
Quantum
140NOC77101


Resolution
This program will read from located registers in Schneider PLC's with the following network modules installed:

  • 140NOC77101
  • BMXNOC0401
  • TSXETC101

Do not use this example to read from located registers in Schneider PLC's through the following network module:
  • 140NOC78000

Attachments
170NOC77101_CIP_Modbus_Object_READ_Example.pdf

Schneider Electric Global

Attachment(s)
170NOC77101_CIP_Modbus_Object_READ_Example.pdf [166.68 KB]