{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Neither Real Time Data Nor N/A Is Displayed In WebReach

Goals and Symptoms

Summary


  • All diagrams load in WebReach, and historical data is retrievable, but no real time data displays. Where values should be updating in the diagrams, nothing is displayed, not even N/A. The operating system is a Windows 2003 Server with Service Pack 1.

    Symptoms

    No real time data is displayed when a WebReach diagram loads; moreover, not even an N/A is displayed. If ShowSubscriptions.asp is used to view handle and data values, then nothing is displayed and Number of Subscriptions is 0. The operating system is likely Windows 2003 Server Service Pack 1.

Facts and Changes

Keywords
WebReach

Real Time

N/A

Windows 2003 Server Service Pack 1

Causes and Fixes

Cause
Internet Explorer browser settings need to be adjusted.

Resolution

Within Internet Explorer, choose Tools/Internet Options and add http://<server name> to the list of trusted sites. See the following screen captures:

Original article#11696


Legacy KB System (APS) Data: RESL182922 V1.0, Originally authored by DaMi on 03/20/2007, Last Edited by DaMi on 03/20/2007
Related ranges: ION Enterprise

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.