{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the part number for the EGX power supply?

Issue
What is the part number for the EGX power supply?

Product Line
EGX100, EGX150, EGX200, EGX300, EGX400

Environment
Installation

Resolution

Power Supply Offering
Schneider Electric sells two 24 Volt power supplies for the EGX gateways:

3090PS24 - 7.5 Watt 24 Volt power supply
PSSVCSPS24V50W - 50 Watt 24 Volt power supply

Additionally, Schneider Electric offers a Power Over Ethernet Injector Kit: TCSEAV0100

Gateway Requirements
EGX200/400 Gateway - Any 24 Volt power supply with a minimum output of 8 Watts is sufficient
EGX100/300 Gateway - Any 24 Volt power supply with a minimum output of 4 Watts is sufficient
EGX150 Gateway - Any 24 Volt power supply with a minimum output of 15 Watts is sufficient

The EGX100/300/150 gateways are also capable of receiving power over ethernet.

The table below indicates the supported power supplies per gateway:

EGX200EGX400EGX100EGX300EGX150
24 Volt24 Volt24 VoltPOE24 VoltPOE24 VoltPOE
3090PS24XX
PSSVCSPS24V50WXXXXX
TCSEAV0100XXX

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.