Goals and Symptoms
Is it possible to take our vigilohm EM9B with the reference number 50557 for voltage 200VAC / 380-800Hz as the frequency range shows in catalog is 50-60-400-1000Hz.
Facts and Changes
Keywords: EM9B, Vigilohm, Frequency range, range of frequencies, operating range, range of operation, frequency spectrum
Causes and Fixes
In catalog, frequency range of EM9B is shown as 50-60-400-1000Hz. This means it will work on all frequencies from 50 to 1000Hz.
Last Revised: 14-Feb-08Public
All content © 1992-2008 Schneider Electric
Legacy KB System (APS) Data: RESL191087 V1.0, Originally authored by KBAdPM on 02/16/2008, Last Edited by KBAdPM on 02/16/2008
Related ranges: Vigilohm
Released for:Schneider Electric Global