Goals and Symptoms
Summary:
Using ION Enterprise 5.6 Service Pack 2 (SP2) on a Windows XP Pro SP3, it is possible that real time data can be updating in Vista, but when Webreach is opened there is no real time data for any meters, just blanks. Repairing MDAC 2.81 has been found to resolve the issue.
Symptoms:
- Real time data in Numeric objects in Webreach show blanks (no N/A or '...')
- All other KB articles for troubleshooting Webreach real time data do not work to resolve this issue.
- No Windows Event log errors
- ION Enterprise Setup log errors can be found to be the cause of real-time data not working.
Facts and Changes
Keywords:
Webreach
Real time Realtime OR Real-time data
Blank OR Blanks
MDAC
Windows XP Pro SP3, SP2
empty boxes
Causes and Fixes
Causes:
Problems with Microsoft's MDAC component in Windows XP.
Fixes:
Follow Method 2 of this Microsoft KB article to repair the MDAC.
http://support.microsoft.com/kb/899861
Excerpt:
|
Attachments
(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/c3888b97d39e39a3c125755b00583202/fl_block_5/0.3070?OpenElement&FieldElemFormat=gif)
- Date Created: December 17, 2008
Last Revised: February 12, 2009
Public
Original Author: EW
All content © 1992-2009 Schneider Electric
Legacy KB System (APS) Data: RESL197797 V1.0, Originally authored by KBAdPM on 02/12/2009, Last Edited by KBAdPM on 02/12/2009
Related ranges: ION Enterprise V5.6
Released for:Schneider Electric Global