Issue:
Writing a new IP address of an Equipment at Runtime in Vijeo Designer
Product Line:
Vijeo Designer
Resolution:
Yes, you can write the IP address of an equipment via scripting. This feature was implemented in Vijeo Designer V5.0 SP1. This code will set IP Addresses for any driver, not just the Modbus driver. Below is an example script:
// --------------- Write some data -----------------------------------------// Length is given by NewIP_InputData.length
-
- int [ ] NewIP_InputData = {10, 187, 225, 135};
ModbusEquipment01.openConfig();
ModbusEquipment01.setProperty( "Con_IPAddress", NewIP_InputData );
ModbusEquipment01.commitConfig();
- int [ ] NewIP_InputData = {10, 187, 225, 135};
-
Released for:Schneider Electric Global