Can the split rear doors of a NetShelter SX, SV or VX cabinet be installed on the front of the cabinet, and can the front door be installed on the rear?
Published date:
16 August 2019
Issue:
Design of the data center may require a full width door on the rear and/or split doors on the front.
Cause:
Data center layout requires NetShelter SX, SV or VX cabinet to be flexible and allow the customer to choose what door style is installed in the front and/or rear.
Resolution:
Yes, the rear doors can be installed onto the front of the cabinet and the front doors onto the rear.
When moving the rear doors to the front you must also move one set of hinges from the rear to the front.
Replacement front and rear door kits include all of the hinges necessary to hang the doors.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.