{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the operating temperature for the ATV61?
Issue:
ATV61 operating temperature specification

Product Line:
ATV61 Altivar 61

Environment:
All

Cause:
Verify application requirements.

Resolution:
Ambient air temperature around the device :
Operation °C
For ATV 61H..... drives: - 10…+ 50 without derating, depending on the rating.  Up to + 60°C with derating (and with control card fan kit VW3 A9 4.. depending on the rating).
For ATV 61W.... drives: - 10…+ 40 without derating.
Storage °C - 25…+ 70

Schneider Electric Global