Issue
May the settings file from a VPG210-001361 be directly loaded into a VAMP 210-5A7ADA-3.20 using VAMPset?
Product Line
VAMP relays
Resolution
If the complete part numbers doesn't match one cannot load the same setting file to each other. Each VAMP relay will have to be manually configured.
Also if the unit has the same part number and firmware is not the same one cannot load the setting file.
Released for:Schneider Electric Global