{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Vijeo Designer will not completely build the project.
Issue:
Vijeo Designer will not completely build the project.

Resolution:

Vijeo Designer will not completely build if there are errors in the project.  The errors will show up in the Feedback Zone window.  Once all of the errors are fixed, build the project again and it clean out the error message.  You should get a message that "Build Complete" in the Feedback Zone.

If you do not see any details of the errors, goto Build menu -> Options -> check the box for "Display Detail during Build" and select OK.  Then build the project again.

NOTE: If your Feedback Zone is not appear on the screen, try pressing SHIFT+F6 to bring the window back. If it is still missing, you may have resized it to the point where it is too small appear on the screen. In this case, you will need to contact Technical Support to reset the window sizes.

Schneider Electric Global