Issue:
Looking for a circuit breaker or fuse that is used with the ATV212 drive.
Product line:
Altivar 212
Environment:
All models, all serial numbers
Cause:
Recommended fuse rating for UL and CSA requirements.
Resolution:
The breaker and fuse sizing can be found in the ATV212 Quick Start Annex. The manual document is S1A7347602.
Looking for a circuit breaker or fuse that is used with the ATV212 drive.
Product line:
Altivar 212
Environment:
All models, all serial numbers
Cause:
Recommended fuse rating for UL and CSA requirements.
Resolution:
The breaker and fuse sizing can be found in the ATV212 Quick Start Annex. The manual document is S1A7347602.
Released for:Schneider Electric Global