{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is the Q suffix on the ATS22 soft starter?

Issue:
Q suffix on the ATS22

Product Line:
ATS22

Environment:
All ATS22 Q suffix version soft starts

Cause:
Can customer use ATS22D32Q on his pumping application

Resolution:
Q Suffix on the ATS22 was designed for the European market.  Our Suggestion would be to use the S6U or S6 suffix version for the US market.
Q Suffix version does not have ground fault protection and its only for available with 460VAC input, 230VAC control voltage and 24vdc logic input control voltage.
Q Suffix Version if you are not going to use inside the Delta wiring you will need to change parameter setting dLtA to LINE.  If you are using inside the delta wiring leave  dLtA to dLT.

Schneider Electric Global

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.