{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the ATV71 Drive comply with functional safety standard EN13849-1?

Issue:
ATV71 functional safety standard EN13849-1 compliance

Product Line:
ATV61 /ATV71

Environment:
All

Cause:
None

Resolution:
Power Removal safety function input is a safe torque off input. When PWR is not connected to the 24V, the motor cannot be started (compliance with functional safety standard EN 954-1, ISO 13849-1 and IEC/EN 61508)

Schneider Electric Global