Issue:
ATS22 does not follow the decel ramp.
Product Line:
Altistart 22 ATS22
Environment:
All ATS22
Cause:
Ramp time is short.
Resolution:
The ATS22 cannot produce braking torque during the deceleration ramp. It can only produce driving torque. Therefore, the deceleration ramp can extend the stopping time by ramping down the driving torque. It cannot reduce the stopping time to less than a normal coast to stop.
When a braking feature is required, use a variable speed drive and consider an optional DB resistor.
Released for:Schneider Electric Global