Why do I get an error, "Error 2010: [Switch] [Logout] [When Touch] invalid selection", after adding a Log out object from the Toolchest.
Published date:
28 March 2019
Title
Why do I get an error, "Error 2010: [Switch] [Logout] [When Touch] invalid selection", after adding a Log out object from the Toolchest.
Issue
To make customers aware that in order to use any security objects from the toolchest. Target security needs to be enabled.
Product Line
Vijeo Designer
Environment
Cause
Resolution
You will get this error message if you do not have security setup for the target and added the Logout object from the Toolchest. Once you enable target security that will resolve the error on the build.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.