Issue:
Need to determine if the NetShelter CX can effect wifi signal strength.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Wireless devices can be installed inside a NetShelter CX cabinet.
Resolution:
A wireless device was tested in the NetShelter CX manufacturing facility. The signal strength was affected by less than 10% in 3 of the test areas and by 38.46% in 1 of the areas. The test results show that the Office had the greatest signal reduction but only dropped to a Fair signal strength. None of the results indicated a poor or unusable signal.
A complete test report is attached below.
Released for:Schneider Electric Global