Issue:
ATV71 firmware revision compatibility with V1.1IE04 of the devicenet card VW3A3309.
Product Line:
Altivar 61 and Altivar 71 series drives.
Environment:
All part numbers, All serial numbers.
Cause:
Some firmware updates are not backwards compatible with legacy versions of current drives.
Resolution:
The minimum control card firmware of an Altivar 61 / 71 series drive that is compatible with revision 1.1IE04 of devicenet card VW3A3309 is 1.1IE04. Previous firmware revisions of the control card are not compatible with this devicenet card.
Released for:Schneider Electric Global