{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
For the Enclosed ATS22, what is the difference between the Basic Shunt Trip and Full-Featured Shunt Trip power circuit options?

Issue:
What is the difference between the Basic Shunt Trip and Full-Featured Shunt Trip versions of the Enclosed ATS22?

Product Line:
Enclosed AST22

Environment:
All models

Cause:
Define features for quoting

Resolution:
The electrical schematics are the same.  The Basic Shunt Trip unit is a space optimized version of the Enclosed 22 controller.  Limited space is provided for field mountable control equipment.  The Full-Featured Shunt Trip unit is a fully customizable version.  Additional space is provided for engineered options and field installable equipment.

Schneider Electric Global