Issue:
ATV12 Profibus communication setup
Product Line:
ATV12
Environment:
All models
Cause:
Network communications options
Resolution:
No, the ATV12 drive does not have a Profibus communication option. It only has the integrated Modbus serial port. Consider a 3rd party gateway to convert between Modbus and Profibus.
Released for:Schneider Electric Global