Issue
Need to modify a CID file using XML
Product Line
CET850
IEC61850
Resolution
CET850 offers an XML source editor, however it is deactivated by default and must be manually activated. To activate; open CET850 and click Tools > Preferences. Located beneath Editing Control check the box next to "Enable XML source editing" to activate this feature.
Once this is enabled to view the CID file in XML, highlight the IED click View > Click XML Source.
Need to modify a CID file using XML
Product Line
CET850
IEC61850
Resolution
CET850 offers an XML source editor, however it is deactivated by default and must be manually activated. To activate; open CET850 and click Tools > Preferences. Located beneath Editing Control check the box next to "Enable XML source editing" to activate this feature.
Once this is enabled to view the CID file in XML, highlight the IED click View > Click XML Source.
Released for:Schneider Electric Global