Issue:
Part number request for the power terminal shrouds for the ATS22 series Soft Starters
Product Line:
ATS22 series soft starters.
Environment:
ATS22C11S6,S6U..C17S6,S6U and ATS22C21S6,S6U..C59S6,S6U All serial numbers.
Cause:
Customer has requested optional terminal shrouds.
Resolution:
For the ATS22C11S6,S6U through ATS22C17S6,S6U, the part number is LA9F702.
For the ATS22C21S6,S6U through ATS22C59S6,S6U, the part number is LA9F703.
The thermal shroud kit includes a set of 6 power terminal protection shrouds.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Global