Issue:
Programming the R1 or R2 on the ATV31/ATV312 drives.
Product Line:
ATV31 or ATV312
Environment:
All
Cause:
Setting up R1 and R2 relays on the ATV31 or ATV312 drives?
Resolution:
Note: "press Enter" means press in on the dial, and "scroll down" means turn the dial clockwise.
- While at RDY on the drive's display, press Enter
- Scroll down to I/O menu and press Enter
- Scroll down to R1, press enter, and choose your desired setting. Example: FLT is drive fault.
- Scroll down to R2 enter and choose your desired setting. Example: RUN is drive running.
For further detail, please refer to page 50 in the ATV312 Programming Manual.
https://www.se.com/ww/en/download/document/BBV46385/
Released for:Schneider Electric Global