Issue
KVM-SERIAL Configuration Information and Assistance including module's DB-9 pinout and general information
Product Line
- Rack Accessories - KVM Switches
- KVM1116P, KVM2116P, KVM2132P
Environment
- All serial numbers
- All firmware versions
- KVM-SERIAL applications
Cause
Typically, when using KVM-SERIAL a gender changer, serial cable, or port configuration is often required. This article is intended to help provide some of that information.
Resolution
Below is the pinout configuration for the KVM-SERIAL server module.
In an example configuration with an APC UPS with a DB-9 port serial port (which uses 940-0024 or 940-1524 APC serial cable for communications), we have connected KVM-SERIAL in the following manner.
Parts used:
- Model KVM1116P KVM Switch
- APC part number KVM-SERIAL server module
- APC Smart UPS 750 (model SUA750, with DB-9 serial port)
- (2) DB-9 gender changers
- (1) part number 940-0024 or 940-1524 APC UPS Smart Signaling serial cable
- (1) part number 940-0103 APC null modem serial cable
- Physical connection: KVM Switch->KVM-SERIAL (DB-9F)->F to M gender changer->940-0103 APC null modem cable->F to M gender changer->940-0024/1524 APC Smart Signaling cable->UPS DB-9F.
- KVM-SERIAL port configuration (set within KVM1116P): 2400 baud rate, 8 data bits, parity none, 1 stop bit, no flow control.