{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Installing firmware update with Spanish language support on PM5350 using DLF-3000 3.3 v2
Issue:
Need to update PM5350 firmware with Spanish language support.

Product Line:
PM5350
DLF-3000

Environment:
Firmware Upgrade

Cause:
Firmware related issue.


Resolution:
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.

*Warning: Be sure all other software, is not connected to the meter.*

Use the following link to download the DLF-3000 software:

DLF-3000 Download

The process for updating a Language Library (LL) is the same as any other DLF-3000 firmware update. The attached tutorial will walk you through how to update the firmware of a PM5350 meter using DLF-3000
software and serial communication:

Schneider Electric Global

Attachment(s)
PM5350 Spanish FW Update through DLF3000 .pdf [1.01 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.