{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum number of variables in Web Designer application for a BMXNOE0110 module.
Issue
What is the maximum number of variables in Web Designer application for a BMXNOE0110 module.

Product Line
BMXNOE0110

Environment
Windows 7

Issue
The maximum number of WORD type variables that can be defined in a Web Designer application for a BMXNOE0110 module is 1000.  If STRING type variables are used, the  device 'Variables' table namespace in a Web Designer application for a BMXNOE0110 module is limited to a total of 2000 bytes.  If the 'Variables' table contains a mixture of WORD and STRING type variables, the limit is still 2000 bytes.   Any attempt to exceed the limit could result in communications issues with the Web Designer services.


This limit is due to the available memory in the module and cannot be changed.

Schneider Electric Global