Can the ATS48 Soft Starter be programmed to run a motor in reverse?
Published date:
01 February 2019
Issue:
Can the ATS48 Soft Starter be programmed for reverse?
Product Line:
ATS48
Environment:
All serial numbers for ATS48
Cause:
N/A
Resolution:
No, the ATS48 Soft Starter cannot be programmed for reverse. If a reverse option is required, use a reversing contactor ahead of the ATS48. Please see Figure 35 in the attached manual for a diagram.