{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the part number for the Ethernet IP / Modbus TCP IP option card for the ATV32 series drives?
Issue:
ATV32 part number for the Ethernet IP/Modbus TCP/IP option card.

Product Line:
Altivar 32 series drives.

Environment:
All models, All serial numbers.

Cause:
Part number unknown.

Resolution:
The part number for the combination Ethernet IP/Modbus TCP/IP card for the Altivar 32 series drives is VW3A3616