{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is RE17RMMW product’s output able to drive 26Vdc 20mA load?

The output of RE17RMMW product is an electromechanical relay. This relay is designed to operate a resistive load.  You may operate a small inductive load if needed. Please take note that, the relay contacts lifespan will reduce when we operated an inductive load.

Attached herewith is the life curves specification of the electromechanical relay component. (Refer to attachment)

Schneider Electric Global

Attachment(s)
Output Specification.pdf [47.93 KB]