{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is a line reactor required with a ATV312 600V drives?
Issue:
ATV312 600V drive requirement of a line reactor.

Product Line:
ATV312  ATV31

Environment :
All  575-600V

Cause:
New installation

Resolution:
Yes, a minimum 3% line reactor is required on all 575V / 600V drive installations.