{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV12 Can you have the run command from remote display and terminals?

Issue:
ATV12 run command in the remote display and the terminals.

Product Line:
Altivar 12

Cause:
Run the drive from 2 command sources

Resolution:
Yes it is possible:
Navigate to ConF- /   FULL- /  CtL- /  FR1 = LCC
Then to CON- / FLO = L1H

This configuration will start the drive from the remote display (the green RUN button) and if we close the contact on LI1.