Open the Unity Pro project. Open an LL984 network.
Go to <Tools> <Project Settings> Program - LL984 - Network Display.
In the panel on the right, Choose View1, for example, as Print view.
On the left, highlight View1.
Edit the Property Labels on the right, starting with Line 7 and working up.
<Apply><OK>.
The type of documentation specified in the View should be reflected in the LL984 network as well as in the networks that are printed.
Go to Documentation in the Project Browser and Choose 'Program' by right clicking and choosing 'Include Heading'.
A red mark will appear to the left of Program.
<File><Print> will print the Ladder Logic in the project.
Released for:Schneider Electric Global