Issue:
Does Vijeo Designer Lite v1.3 run on Windows 7 64bit OS?
Product Line:
Vijeo Designer Lite
Environment:
Legacy HMI Configuration Software for XBTN, XBTRT family Human Machine Interfaces (HMI)
Resolution:
No, Vijeo Designer Lite v1.3 does not support Windows 7 64bit.
Vijeo Designer Lite v1.3 is only supported on Windows XP and Windows 7 32-bit OS.
No, Vijeo Designer Lite v1.3 does not support Windows 7 64bit.
Vijeo Designer Lite v1.3 is only supported on Windows XP and Windows 7 32-bit OS.
Released for:Schneider Electric Global