Issue:
Adjusting the high speed to go above 60Hz on the ATV61 and ATV71 drives
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Needs to adjust the high speed above 60Hz
Resolution:
WARNING: Setting these parameters too high for your motor could cause motor damage and personal injury. Consult your motor's manufacturer before performing these steps to be sure it's safe for your motor to run above 60Hz and for how long.
In the Simply Start Menu 1.1:
- Set max frequency (fFr) to to desired value
- Set high speed (HSP) to desired value
Released for:Schneider Electric Global