{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you read over modbus if the ATV61 or ATV71 drive is in local or remote control mode with the F4 function key?

Issue:
ATV61 or ATV71 drive is in local or remote control mode with the F4 function key reading over modbus?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to know if the F4 function key is in local or remote mode.

Resolution:
I suggested he monitor Address 8441 or 8442 bit 2 to show graphic display command or reference.
This bit 2 will go high when in local HMI mode.

Schneider Electric Global

Attachment(s)
atv61_parameters_en_v4.pdf [3.26 MB]