{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you program the ATV61 and ATV71 drive to start stop with the HMI and use AI2 for 4-20mA speed control?

Article available in these languages: Spanish

Issue:
Configuration the ATV61 and ATV71 drive to start stop with the HMI and use AI2 for 4-20mA speed control.

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Wants to start and stop the drive with his remote keypad display and use his 4-20mA signal for speed control.

Resolution:
Program the drive as follows
Drives MENU
Simply Start Menu 1.6
Ref 1 channel is AI2
Profile is set to SEP ( Separate)
CMD switching set to Channel 1 active
CMD channel 1 set to HMI

Schneider Electric Global

Attachment(s)
ATV61 Prog Jun 07 1760649.pdf [6.84 MB]