Issue:
ATV212 Profibus communication
Product Line:
ATV212
S-Flex enclosed ATV212
Environment:
All models and serial numbers
Cause:
None
Resolution:
Profibus is not offered as a communication option.
There are several third party companies such as "Anybus" that may be able to provide a gateway option from Profibus to one of the ATV212 integrated protocols (Modbus, BACnet, Metasys N2, or Siemens P1).
Released for:Schneider Electric Global