{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Does the ATV312 drive come with a remote keypad?

Issue:
Is a remote keypad come with the ATV312 drive as standard?

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The ATV312 drive does not come with a remote keypad as a standard item.  It must be ordered separately.
Remote Keypad Display
(IP54) ATV312, ATV12 VW3A1006
(IP65) ATV312, ATV12 VW3A1007
Mounting Kit, VW3A31101
Graphic Display  (used also with ATV61 and ATV71)  VW3A1101

Schneider Electric Global