Issue:
What are the part numbers of the terminal block for the BMXAMI0800?
Product Line:
X80 I/O Modules
Resolution:
There are 2 types of terminal blocks for the BMXAMI0800. Cage clamp-type part number BMXFTB2800 or Spring-type part number BMXFTB2820.
What are the part numbers of the terminal block for the BMXAMI0800?
Product Line:
X80 I/O Modules
Resolution:
There are 2 types of terminal blocks for the BMXAMI0800. Cage clamp-type part number BMXFTB2800 or Spring-type part number BMXFTB2820.
Released for:Schneider Electric Global