{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the HDMPMHKIT27 wiring harness be used to add additional meters to an HDM enclosure?
Issue
A user would like to install additional meters into a HDM meter cabinet.

Product Line
PowerLogic® High Density Metering

Environment
HDM Enclosures Meter Installation

Cause
An auxiliary harness is needed to install additional meters in a HDM enclosure.

Resolution
The Auxiliary Harness Assembly Kit is used when adding a new row of meters to the metering cabinet in the PowerLogic® High Density Metering System.
The auxiliary harness accommodates up to four meters and is used in rows 2, 3, or 4 depending on the number of meters installed and the model of the cabinet.

The Auxiliary Harness Assembly Kit Instruction Bulletin is attached to this article.

Schneider Electric Global

Attachment(s)
Auxiliary_Harness_Assembly_Kit_63230-504-203A1.pdf [782.54 KB]