Issue:
Wondering what is the effect of altitude on ATV312 drives?
Product Line:
All ATV312 and ATV31
Environment:
High altitude, more than 1000m
Cause:
Installing the drive in high altitude above sea level.
Resolution:
For all ATV312, less than 1000m, no derating.
For single-phase supplies and corner grounded distribution networks, up to 2000m, derating 1% per 100m.
For three-phase supplies, up to 3000m, derating 1% per 100m.
Released for: Schneider Electric Global