{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the output voltage from the ATV212 RYA-RYC contact?
Issue:
Needs the output voltage from the ATV212 RYA-RYC contact

Product Line:
Altivar 212 ATV212

Environment:
All

Cause:
Status indication feedback

Resolution:
There is no drive output voltage from the RYA-RYC contact.  This is a dry contact.

Specs are as follows:
Minimum switching capacity: 3mA for 24Vdc
Maximum switching capacity:
resistive load 3A for 250Vac or 30Vdc
inductive load 2A for 250Vac or 30Vdc
Maximum response time: 7msec +- 0.5msec