Issue:
PT100 probe to measure temperature
Product Line:
ATV61 and ATV71
Environment:
All models and serial numbers
Cause:
None
Resolution:
No, LI6 is a digital input and cannot read a resistance or an analog value. LI6 can be used in conjunction with a PTC. The input is activated when the resistance of the PTC reaches 3k ohms.
It is not designed to accept a PT100 probe.
ATV630 can do this.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global