Issue:
Instructions on how to set up STO, SS1 and SLS safety inputs on the ATV32.
Environment:
Altivar ATV32
Cause:
All
Resolution:
There are three safe inputs that can programmed on the ATV32 drives.
STO= means Safe Torque Off
SS1= means Safe Stop 1
SLS= means Safely-limited speed
These inputs can only be assigned or programmed using SoMove software
Basic instructions Open SoMove software
You will need to connect the drive before you assign any of the safety inputs.
Choose the Safety function TAB
Choose configure
Type in your password or 6969 enter
Choose one of two inputs SLS or SS1 and assign them to a logic input or assign STO.
See the attached files for assistance.
Program application and programming assistance see the S1A45606 safety manual
Instructions on how to set up STO, SS1 and SLS safety inputs on the ATV32.
Environment:
Altivar ATV32
Cause:
All
Resolution:
There are three safe inputs that can programmed on the ATV32 drives.
STO= means Safe Torque Off
SS1= means Safe Stop 1
SLS= means Safely-limited speed
These inputs can only be assigned or programmed using SoMove software
Basic instructions Open SoMove software
You will need to connect the drive before you assign any of the safety inputs.
Choose the Safety function TAB
Choose configure
Type in your password or 6969 enter
Choose one of two inputs SLS or SS1 and assign them to a logic input or assign STO.
See the attached files for assistance.
Program application and programming assistance see the S1A45606 safety manual
Released for:Schneider Electric Global