Issue
When troubleshooting database issues, gathering some basic information can be very helpful in leading to the resolution or to identifying the cause of problems.
Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Power Monitoring Expert Software with SQL Server 2005-2022 versions
Cause
Database maintenance and troubleshooting possible database issues.
Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
Listed below are three methods to find the last time SQL Server server/service was restarted.
Method 1
The first method uses the fact that 'tempdb' will be recreated with every restart. We can check the created date (crdate) from master..sysdatabases.
SELECT crdate FROM master..sysdatabases WHERE name ='tempdb'
Method 2
The second method checks the master..sysprocesses database and check for the minimum value in the 'login_time' column.
SELECT MIN(login_time) FROM master..sysprocesses
Method 3
Examine the Windows Event Viewer and search for the most recent event indicating that the SQL server service was started.
- Right click on the Start button and select Control Panel > System & Security and double-click Administrative tools
- Double-click Event Viewer
- Select the type of logs that you wish to review (ex: Application, System)
NOTE: To access the Application Logs once in Event Viewer, go to Windows Logs > Application, for shutdown errors refer to Application and System logs.
Released for:Schneider Electric Global