{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where can I find information on the ATV212 Modbus communication, specifically related to the RJ45 and the screw terminals pin outs?

Article available in these languages: Spanish

Issue:
ATV212 Modbus RJ45 and the screw terminals pin outs

Product Line:
Altivar ATV212, Sflex 212 SFD212

Resolution:
See the attached file
RJ45 connector
Pin 4= + DB or D1
Pin 5= - DA or DO
Pin 8= com

Screw terminals
B= +
A= -
GND= common
SCR= shield

The complete Modbus manual for the ATV212 products is downloadable from this link: https://www.se.com/us/en/download/document/S1A53844/

Schneider Electric Global

Attachment(s)
ATV212 RJ45 and screw terminal connections.pdf [106.1 KB]