{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Prima P / what is the spacing rods 04691 kit composition / dimensions
The 04691 kit is composed of Insulated threaded parts made of Epoxy glass:
1 rod M10, length 475mm + 2 square nuts (thickness 10mm for a 17mm tool)
Also included: 3 thermoplastic tubes diameters int./ext: 12mm/30mm - length 60mm.
And 2 metallic washers (thickness1.6mm)

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.